The UCI Tx sequence window displays the
currently configured UCI transmission sequence. The UCI channel cannot
be transmitted in subframes occupied by UL-SCH processes. (In the Channel Setup
node, set the UL-SCH State to Off, if necessary.) You can set parameters
for each UCI transmission from within the UCI Tx sequence window. Click
the button
to access a drop-down list
that enables you to set parameters for all UCI Tx sequences to the same
value. The configured parameters are displayed in the Tx Map.
UCI Tx sequence window